AXIS#.SAFEPARAM.SAR_#.ACCLOWERLIMIT

Description

Indicates the acceleration lower limit of the Safe Acceleration Range (SAR) safety function.

 

Parameters Editor with Acceleration Lower Limit setting circled

This is a_LL_SAR in the following diagram:

Context

For complete SAR information refer to SAR (Safe Acceleration Range).

Related safety parameters:

Versions

Action Version Notes

Implemented

02-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Depends on user units

Range

[-2^31+1, 2^31-1]

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SAR_1.ACCLOWERLIMIT

3166h

05h

Signed32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SAR_2.ACCLOWERLIMIT

3167h

05h

Signed32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SAR_3.ACCLOWERLIMIT

3168h

05h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SAR_1.ACCLOWERLIMIT

3266h

05h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SAR_2.ACCLOWERLIMIT

3267h

05h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SAR_3.ACCLOWERLIMIT

3268h

05h

Signed32

-

-

Read/Write

No